CMP#.SOURCEVAL

Description

CMP#.SOURCEVAL is the sampled value of the compare channel source. It reports the value before the channel’s modulo function is applied if CMP#.MODEN = 1. Its scaling depends on CMP#.SOURCE.

  CMP#.MODEN
0 1
CMP#.SOURCE 1-10

FB#.P without modification

FB#.P with modulo

11-12

AXIS#.PL.FB without modification

AXIS#.PL.FB with modulo

Examples

Usage

Code

The following commands read the values for channel 1 and channel 2. In this example the units for CMP1.SOURCEVAL are deg, and the units of CMP2.SOURCEVAL are feedback counts.

--> CMP1.SOURCE 12
--> AXIS1.UNIT.PROTARY 2
--> CMP1.SOURCEVAL
-749.205
--> CMP2.SOURCE 3
--> CMP2.SOURCEVAL
493626.000

Context

For more information please refer to Compare.

Versions

Action Version Notes
Implemented 02-06-00-000  

General Information

Type

Read Only

Units

Depends upon CMP#.SOURCE

Range

Full Position Range

Default Value

N/A

Data Type

Float

See Also

 

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.